Solid Edge Draft Type Library
DisplayHScroll Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
SheetWindow Object
: DisplayHScroll Property
Description
Specifies whether or not the horizontal scroll bar is displayed.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayHScroll As Boolean
Remarks
If True, the scroll bar is displayed.
See Also
SheetWindow Object
|
SheetWindow Members
Send comments
on this topic.