Solid Edge Draft Type Library
ArrangeDimensionsInSelectSet Method
Sets the stack pitch for dimension.
If "True" then function will create associative groups of selected dimensions.
Description
Arranges the dimensions in the select set. API SolidEdgeDraft.DrawingView.AddConnectedDimensionsToSelectSet() can be used to add dimensions to select set which are connected to DV
Syntax
Visual Basic
Public Sub ArrangeDimensionsInSelectSet( _
   ByVal iStackPitchMultiplier As Double, _
   ByVal bAssociative As Boolean _
) 
Parameters
iStackPitchMultiplier
Sets the stack pitch for dimension.
bAssociative
If "True" then function will create associative groups of selected dimensions.
Example
Imports System.Runtime.InteropServices
Public Class DimensionAutoArrange

    Private Sub btnDimensionAutoArrange_Click(sender As System.Object, e As System.EventArgs) Handles btnDimensionAutoArrange.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim ObjDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing
        Dim objType As Type = Nothing

        Try

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If

            ObjDraftDocument = objApplication.ActiveDocument

            'getting the Active Sheet object
            objSheet = ObjDraftDocument.ActiveSheet

            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingViews(1)

            'Add dimensions to select set which are connected to Drawing View.
            objDrawingView.AddConnectedAnnotationsToSelectSet()

            'Arrange the dimensions in select set.
            objSheet.ArrangeDimensionsInSelectSet(1, False)

            If Not ObjDraftDocument Is Nothing Then
                ObjDraftDocument.Close(False)
                ObjDraftDocument = Nothing
            End If
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub

End Class
See Also

Sheet Object  | Sheet Members

Send comments on this topic.