Solid Edge Draft Type Library
ViewPlane Object
Members 
Description
Provides methods and properties that extend to an auxiliary DrawingView object.
Object Model
ViewPlane ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDrawingView ObjectApplication ObjectBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView Object
Remarks
These methods and properties provide information and controls for the display and characteristics (such as text color) of the view plane's caption, the view plane line type and line width, the view plane terminator ratio and type, and so forth. The ViewPlane methods and properties extend to a DrawingView object whose type is igAuxiliaryView, through the DrawingView.Annotation property. An auxiliary DrawingView object is created with the AddByAuxiliaryFold method of the DrawingViews collection object.
See Also

ViewPlane Members

Send comments on this topic.