Solid Edge File Properties Object Library
Count Property
Description
Number of properties in this property set
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objPropertySets As SolidEdgeFileProperties.PropertySets = Nothing
        Dim objProperties As SolidEdgeFileProperties.Properties = Nothing
        Dim iCount As Integer

        Try
            ' Create a new instance of PropertySets.
            objPropertySets = New SolidEdgeFileProperties.PropertySets
            objPropertySets.Open("C:\Part1.par", True)
            objProperties = objPropertySets.Item("Custom")
            iCount = objProperties.Count
            objPropertySets.Close()
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objProperties Is Nothing) Then
                Marshal.ReleaseComObject(objProperties)
                objProperties = Nothing
            End If
            If Not (objPropertySets Is Nothing) Then
                Marshal.ReleaseComObject(objPropertySets)
                objPropertySets = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IJProperties Collection  | IJProperties Members

Send comments on this topic.