Solid Edge File Properties Object Library
Save Method
Description
Save changes made to this property set
Syntax
Visual Basic
Public Sub Save() 
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objPropertySets As SolidEdgeFileProperties.PropertySets = Nothing
        Dim objProperties As SolidEdgeFileProperties.Properties = Nothing
        Dim objProperty As SolidEdgeFileProperties.Property = Nothing

        Try
            ' Create a new instance of PropertySets.
            objPropertySets = New SolidEdgeFileProperties.PropertySets
            objPropertySets.Open("C:\Part1.par", False)
            objProperties = objPropertySets.Item("Custom")
            objProperty = objProperties.Add("My Custom Property", "My Custom Value")
            objPropertySets.Save()
            objPropertySets.Close()
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objProperties Is Nothing) Then
                Marshal.ReleaseComObject(objProperties)
                objProperties = Nothing
            End If
            If Not (objPropertySets Is Nothing) Then
                Marshal.ReleaseComObject(objPropertySets)
                objPropertySets = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IJProperties Collection  | IJProperties Members

Send comments on this topic.