Solid Edge Part Type Library
AssemblyWeldment Object Members
Overview 
Public Methods
Public Method BindKeyToWeldPartModelReturns a model corresponding to the input reference key.
Public Method BindWeldPartModelToKeyReturns a reference key from the assembly occurrence corresponding to the input model.
Public Method EditByDocumentSpecifies the assembly document to edit based on the input document.
Public Method EditByFileSpecifies the assembly document to edit based on the input file name.
Public Method GetRangeByModelReturns the range of a part occurrence specified by an input model.
Public Method GetStyleByModelReturns an object that describes the style of the referenced feature.
Public Method SetStyleByModelSets style of a part occurrence on the referenced object, specified by the input weld part model.
Public Method UpdateLinkUpdates the links in the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property GetEdgesByModelReturns the edges of a part occurrence specified by the input model.
Public Property GetFacesByModelReturns the faces of a part occurrence specified by the input model.
Public Property GetFacesByModelAndRayReturns the faces of a part occurrence specified by the input model and a ray.
Public Property LinkStatusReturns the status of the links for the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
See Also

AssemblyWeldment Object

Send comments on this topic.