| Solid Edge Part Type Library : AttachedPropertyTable Object |
AddMembers | Attaches the referenced AttachedPropertyTable to a specified set of objects. |
AttachedTo | Returns the objects to which the AttachedPropertyTable object is attached. |
Delete | |
RemoveMembers | Removes the referenced AttachedPropertyTable object from the objects in the RemovedAttachments array. |
SelectFilter | Returns the array of filters applied to the array of objects to which the referenced AttachedPropertyTable object is attached. |
Application | Returns the active application object. |
AttachedProperties | Returns the AttachedProperties object for the referenced AttachedPropertyTable object. |
Definition | Sets and returns the PropertyTableDefinition obect for the referenced AttachedPropertyTable object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Name | Returns the name of the referenced object. |
NumAttachedObjects | Returns the number of objects that are attached to the referenced AttachedPropertyTable object. |
Parent | Returns the parent object for the referenced object. |
SystemName | This read-only String property returns the system name for the referenced object. |