|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  CrossSectionType | The shape of the cross section of a Bead.  Circular, U shaped, or V shaped. | 
|  DieRadius | The radius of the rounding applied to the die side of the feature. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  EndCondition | The end treatment applied to an open profile Bead. Formed, Lanced, or Punched | 
|  EndPunchWidth | The width of a punched end Bead. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  FormRadius | The radius of a Circular or V shaped Bead. | 
|  Height | The height of the Bead. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelingModeType |  | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Profile | Sets and returns the Profile object used to construct the referenced feature object. | 
|  PunchRadius | The radius of the rounding applied to the punch side of the feature. | 
|  RoundingOption | Whether or not to apply rounding to the Bead feature. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Side | The side of offset of the Bead with respect to the Plate on which it resides. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  TaperAngle | The angle of the sides of a U shaped or V shaped Bead. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. | 
|  Width | The width of a U shaped Bead. |