| Solid Edge Part Type Library : ComponentSketch Object |
Delete | Deletes the referenced object. |
Application | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | |
Profiles | Returns the Profiles collection object. |
ShowSketchColors | Specifies whether the sketch colors or the element colors are displayed for the referenced object. |
Style | Returns the style for the referenced object. |
Type | Specifies the type of the object being referenced. |