| Solid Edge Part Type Library : ContourFlange Object | 
|  Delete | Deletes the referenced object. | 
|  GetDimensions | Returns the Dimensions collection object for the referenced object. | 
|  GetExtentKeyPoint | |
|  GetProfiles | Returns the profiles associated with the referenced feature object. | 
|  GetStyle | Returns the feature style. | 
|  Range | Returns the high and low range values for the referenced object. | 
|  Reorder | Inserts the referenced object in front of or behind another feature. | 
|  RollToFeature | Rolls the referenced Model object back to a specified feature. | 
|  SetExtentEdgeChain | |
|  SetExtentFinite | |
|  SetExtentToEndOfEdge | |
|  SetExtentToKeyPoint | |
|  SetProfiles | Sets the profiles associated with the referenced feature object. | 
|  SetStyle | Sets the feature style. | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BendRadius | Sets and returns the inside radius of the bend. | 
|  BendReliefDepth | Sets and returns the depth of the bend relief for the specified object. | 
|  BendReliefType | Sets and returns a constant that specifies the Bend relief type. | 
|  BendReliefWidth | Sets and returns the width of the bend relief. | 
|  ChainedEdges | |
|  CloseCornerDiameter | |
|  CloseCornerType | |
|  CornerReliefType | Property That Specifies The Corner Relief Type To Be Used | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  ExtendBendRelief | |
|  ExtentDistance | |
|  ExtentSide | Sets and returns the reference plane side for the referenced object. | 
|  ExtentType | Sets and returns the extent type for the referenced object. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  MitreAngleAtEnd | |
|  MitreAngleAtStart | |
|  MitreBendEdgesLargerThanDefaultBendRadius | |
|  MitreCutType | |
|  MitrePosition | |
|  MitreSideAtEnd | |
|  MitreSideAtStart | |
|  MitreTypeAtEnd | |
|  MitreTypeAtStart | |
|  Name | Returns the name of the referenced object. | 
|  NeutralFactor | Sets and returns the neutral factor applied to the bend. If the UseGlobalNeutralFactor property is True, the global neutral factor is associatively applied, and this local value is ignored. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Profile | Sets and returns the Profile object used to construct the referenced feature object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  UseGlobalBendRadius | Specifies whether or not the global bend radius is to be applied to the referenced object. | 
|  UseGlobalBendReliefDepth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. | 
|  UseGlobalBendReliefWidth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. | 
|  UseGlobalNeutralFactor | Specifies whether or not the global neutral factor is to be applied to the referenced object. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |