|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Axis | Sets and returns the Axis object about which the referenced object revolves. | 
|  CoordinateSystemType | Returns the type of the Coordinate System. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelingModeType | Returns the modeling mode of the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  OffsetType | Offset about Global or Relative to other Coordinate System | 
|  Parent | Returns the parent object for the referenced object. | 
|  Plane | For dimensions, returns the planar object used by the dimension to measure an object.  For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. | 
|  RotationType | Rotate about Self or Global | 
|  Status | Returns the status of the specified object. | 
|  Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |