Solid Edge Part Type Library
InternalBoundary Property
Description
Property of copy surface removal of internal boundary option.
Property type
Read-write property
Syntax
Visual Basic
Public Property InternalBoundary As CopySurfaceInternalBoundaryConstants
Remarks
Internal boundary removal is allowed for any face regardless of type or number selected. The only boundaries removed are those that have no stitched surfaces following the copy operation.
See Also

CopySurface Object  | CopySurface Members

Send comments on this topic.