|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  CutDirection | Sets and returns the direction, with respect to the CuttingSurface, toward the portion of the part model that will be divided to form a new DividedPart. | 
|  CuttingSurface | Sets and returns a Face or RefPlane object whose intersection with the part model defines the dividing boundary for the referenced DividePart object. | 
|  DocumentName | Sets and returns the name of the full-path specification of the PartDocument name that contains the referenced DividedPart or FamilyMember object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Order | Returns the order of the curve for the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Status | Returns the status of the specified object. | 
|  Type | Specifies the type of the object being referenced. |