Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfArr(1 To 2) As SolidEdgePart.Profile
Dim objModel As SolidEdgePart.Model
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
Dim objDrfts As SolidEdgePart.Drafts
Dim ObjFaceArr(1 To 4) As Object
Dim objFaces As Object
Dim objDftPln As SolidEdgePart.RefPlane
Dim objDft1 As SolidEdgePart.Draft
Dim objDft2 As SolidEdgePart.Draft
Dim lngStatus As Long
Dim dblAngArr(1 To 4) As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Draw the Profile
Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
Set objLines = objProfArr(1).Lines2d
Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.06, y2:=0)
Call objLines.AddBy2Points(x1:=0.06, y1:=0, x2:=0.06, y2:=0.06)
Call objLines.AddBy2Points(x1:=0.06, y1:=0.06, x2:=0, y2:=0.06)
Call objLines.AddBy2Points(x1:=0, y1:=0.06, x2:=0, y2:=0)
' Relate the Lines to make the Profile closed
Set objRelns1 = objProfArr(1).Relations2d
Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
' Check for the Profile Validity
lngStatus = objProfArr(1).End(ValidationCriteria:=igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Profile not closed")
End If
' Create the Base Protrusion Object
Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
ProfileArray:=objProfArr, profileplaneSide:=igRight, _
ExtrusionDistance:=0.02)
objProfArr(1).Visible = False
' Check the status of Base Feature
If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
MsgBox ("Error in the Creation of Base Protrusion Feature object")
End If
' Create an Array of Faces and DraftPlane
Set objDftPln = objDoc.RefPlanes(1)
Set objFaces = objModel.ExtrudedProtrusions(1).SideFaces
Set ObjFaceArr(1) = objFaces(1)
Set ObjFaceArr(2) = objFaces(2)
Set ObjFaceArr(3) = objFaces(3)
Set ObjFaceArr(4) = objFaces(4)
' Create the Draft Angle Array
dblAngArr(1) = 45 * (PI) / 180
dblAngArr(2) = 45 * (PI) / 180
dblAngArr(3) = 45 * (PI) / 180
dblAngArr(4) = 45 * (PI) / 180
' Create a Draft collection object
Set objDrfts = objModel.Drafts
' Create a Draft
Set objDft1 = objDrfts.Add(DraftPlane:=objDftPln, NumberOfFaceSets:=4, _
FaceSetArray:=ObjFaceArr, _
DraftAngleArray:=dblAngArr, _
DraftSide:=igOutside)
' Check the status of Base Feature
If objDft1.Status <> igFeatureOK Then
MsgBox ("Add method of Drafts object failed")
End If
' Assign the Draft object to another object usig Item method
Set objDft2 = objDrfts.Item(1)
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objModel = Nothing
Set objRelns1 = Nothing
Set objLines = Nothing
Set objProfArr(2) = Nothing
Set objProfArr(1) = Nothing
Set objDrfts = Nothing
Set objDft1 = Nothing
Set objDft2 = Nothing
Set objDftPln = Nothing
Set ObjFaceArr(1) = Nothing
Set ObjFaceArr(2) = Nothing
Set ObjFaceArr(3) = Nothing
Set ObjFaceArr(4) = Nothing
Set objFaces = Nothing
End Sub