Solid Edge Part Type Library
AddFiniteMulti Method
Specifies the number of profiles on which the Extruded feature is to be based.
Contains the Profile objects to be used to construct the feature.
A member of the FeaturePropertyConstants constant set that indicates the direction in relation to the reference plane, in which the extruded feature extends. For example, this argument specifies if an extruded protrusion extends to the positive, negative, or both directions of the profile's reference plane.
Specifies the depth of the extruded feature.
Description
Adds a multi-profile 3-D feature object to an object collection.
Syntax
Visual Basic
Public Function AddFiniteMulti( _
   ByVal NumberOfProfiles As Long, _
   ByRef ProfileArray() As Object, _
   ByVal ProfilePlaneSide As FeaturePropertyConstants, _
   ByVal Depth As Double _
) As ExtrudedCutout
Parameters
NumberOfProfiles
Specifies the number of profiles on which the Extruded feature is to be based.
ProfileArray
Contains the Profile objects to be used to construct the feature.
ProfilePlaneSide
ValueDescription
igAddRound
igAll
igAlongAnAxis
igAngularDummy
igAsConstruction
igBend
igBendAndFaceCornerRelief
igBendOnlyCornerRelief
igBothFeature Properties - Both
igChainedCornerRelief
igChamfer2Setbacks
igChamfer45degSetback
igChamferAngleSetback
igCircular
igCloseCornerCircleCutout
igCloseCornerClosed
igCloseCornerNone
igCloseCornerOpen
igClosed
igCloseFaces
igConcave
igConstantRadiusArc
igConstRadiusRound
igContinuous
igConvex
igCopy
igCornerRound
igCounterboreHole
igCounterboreProfileIsAtBottom
igCounterboreProfileIsAtTop
igCounterdrillHole
igCountersinkHole
igCurvatureContinuous
igCurveSetSeperator
igDeleteFaceHeal
igDelSMFaceBoth
igDelSMFaceNone
igDelSystemRelief
igDelZeroBendRadius
igDevelopableSurface
igEdgeBasedCrossSection
igEdgesByLoop
igEdgesByVertex
igEnd
igEndCaps
igEqualOffset
igEquationType
igExtendFeature Properties - Extend
igExtendBendRelief
igFacesTouchingCurvesOnly
igFilletBendRelief
igFinite
igFlangeCenterOfEdge
igFlangeEndFromEndEdge
igFlangeEndOnEndEdge
igFlangeFromBothEndsOfEdge
igFlangeFromDefinedStartPoint
igFlangeFullEdge
igFlangeMatchFace
igFlangeOffset
igFlangeStartFromEndEdge
igFlangeStartOnEndEdge
igFlatten
igFormedEnd
igFromNonReferenceEnd
igFromReferenceEnd
igFromTo
igFull
igGroove
igHemTypeCenteredLoop
igHemTypeClosed
igHemTypeClosedLoop
igHemTypeCurl
igHemTypeOpen
igHemTypeOpenLoop
igHemTypeSFlange
igIgnoreBlends
igInsideFeature Properties - Remove/Add Material Inside
igInsideDimension
igIntersect
igLancedEnd
igLeftFeature Properties - Project to Left
igLinear
igLinearCurvatureContinuousExtension
igLinearTangentExtension
igLip
igLouverFormedEndType
igLouverLancedEndType
igLouverRound
igLouverRoundNone
igMitreByAngle
igMitreByDist
igMitreManufacturingCut
igMitreNormalToThickness
igMitreParallelToThickness
igMitreRegularCut
igMove
igMultipleEdges
igNatural
igNeutralFactorFromExcel
igNFType
igNoCornerRound
igNoExtendFeature Properties - Do Not Extend
igNone
igNonSymmetric
igNormal
igNormalSideDummyFeature Properties - Normal Side
igNoRound
igNullConstant
igOffset
igOutsideFeature Properties - Remove/Add Material Outside
igOutsideDimension
igOverlapFaces
igParallelDummy
igParallelToPlane
igPartingFromCurve
igPartingFromEdge
igPartingFromPlane
igPartingFromSurface
igPatternAlongCurve
igPatternCircular
igPatternFillRegion
igPatternMirror
igPatternMountingBoss
igPatternRectangular
igPatternUserDefined
igPeriodic
igProfileBasedCrossSection
igProjectOptionProject
igProjectOptionWrap
igPunchedEnd
igRadial
igRaisedCounterboreSlot
igRecessedCounterboreSlot
igRecreateBlends
igRectangularBendRelief
igReflective
igRegularHole
igRegularSlot
igRegularThread
igRemoveBoundaries
igRemoveExternalBoundaries
igRemoveInternalBoundaries
igReverseNormal
igReverseNormalSideDummyFeature Properties - Reverse Normal Side
igRightFeature Properties - Project to Right
igRipBendRelief
igRipCornerRelief
igRndCapAcrossSharpEdges
igRndMiterAtCorner
igRndPreserveTopologyOff
igRndPreserveTopologyOn
igRndRollAcrossSharpEdges
igRndRollAcrossTangentEdgesOff
igRndRollAcrossTangentEdgesOn
igRndRollAlongBlendEdgesOff
igRndRollAlongBlendEdgesOn
igRndRollAroundCorner
igRoundAllVertexSetback
igRoundEndVertexEdgeSetback
igRoundSetbackIsAbsolute
igRoundSetbackIsRelative
igRoundSingleVertexSetback
igRoundStartVertexEdgeSetback
igRoundVertexEdgeSetback
igShowBoundaries
igSideInfoSetSeperator
igSingleEdge
igSMClearanceCutout
igSMFaceCutout
igSMMidPlaneCutout
igSplit
igSplitAngle1Left
igSplitAngle1Right
igSplitDraft
igStart
igStepDraft
igStepDraftPerpendicular
igStraightPipeThread
igSubtract
igSweepAlignArcLength
igSweepAlignNormal
igSweepAlignParallel
igSweepAlignParametrically
igSweepC1Continuity
igSweepC2Continuity
igSweepMergeAll
igSweepMergeAlongPath
igSweepMergeNone
igSweepScaleNone
igSweepScaleStartAndEnd
igSweepTwistNone
igSweepTwistStartAndEnd
igSweepTwistTurns
igSweepTwistTurnsPerUnitLength
igSymmetricFeature Properties - Symmetric Extent
igTangent
igTangentInterior
igTaperByAngle
igTaperByRatio
igTaperByRLRatio
igTaperDimAtBottom
igTaperDimAtTop
igTaperedEnd
igTaperedHole
igTaperedPipeThread
igTaperedToPlane
igTappedHole
igThickness
igThkInProfilePlane
igThkNormalToProfilePlane
igThreeHundredAndSixty
igThroughAll
igThroughAxis
igToEndOfEdge
igToggleToConstructionToggle from Design to Construction
igToggleToDesignToggle from Construction to Design
igToKeyPoint
igToNext
igTreatmentCircleCutout
igTreatmentCrown
igTreatmentDraft
igTreatmentFormedFeatureDisplayAsCenterMark
igTreatmentFormedFeatureDisplayAsModeled
igTreatmentFormedFeatureDisplayAsSketch
igTreatmentFormedFeatureDisplayAsSketchAndCenterMark
igTreatmentIntersect
igTreatmentMiterRelief
igTreatmentOff
igTreatmentRectangularCutout
igTreatmentUCutout
igTreatmentVCutout
igUnequalOffset
igUnite
igUShaped
igVarRadiusRound
igVBottomDimToFlat
igVBottomDimToV
igVShaped
igWeldGrooveCapProject
igWeldGrooveCapSameAsTop
igWeldGrooveCapSurface
A member of the FeaturePropertyConstants constant set that indicates the direction in relation to the reference plane, in which the extruded feature extends. For example, this argument specifies if an extruded protrusion extends to the positive, negative, or both directions of the profile's reference plane.
Depth
Specifies the depth of the extruded feature.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProf As SolidEdgePart.Profile
    Dim objProfile(1 To 2) As SolidEdgePart.Profile
    Dim objExtCut As SolidEdgePart.ExtrudedCutout
    Dim objModel As SolidEdgePart.Model
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLines1 As SolidEdgeFrameworkSupport.Lines2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
    Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
    Dim objRefPln As SolidEdgePart.RefPlane
    Dim objProfCollection As SolidEdgePart.Profiles
    Dim objProfArray(1 To 2) As SolidEdgePart.Profile
    Dim lngStatus As Long
    Dim i As Integer
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Draw the Base Profile
    Set objProfile(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(3))
    Set objLines = objProfile(1).Lines2d
    Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.08, y2:=0)
    Call objLines.AddBy2Points(x1:=0.08, y1:=0, x2:=0.08, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.08, y1:=0.06, x2:=0.064, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.064, y1:=0.06, x2:=0.064, y2:=0.02)
    Call objLines.AddBy2Points(x1:=0.064, y1:=0.02, x2:=0.048, y2:=0.02)
    Call objLines.AddBy2Points(x1:=0.048, y1:=0.02, x2:=0.048, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.048, y1:=0.06, x2:=0.032, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.032, y1:=0.06, x2:=0.032, y2:=0.02)
    Call objLines.AddBy2Points(x1:=0.032, y1:=0.02, x2:=0.016, y2:=0.02)
    Call objLines.AddBy2Points(x1:=0.016, y1:=0.02, x2:=0.016, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.016, y1:=0.06, x2:=0, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0, y1:=0.06, x2:=0, y2:=0)
    ' Define Relations among the Line objects to make the Profile closed
    Set objRelns = objProfile(1).Relations2d
    Call objRelns.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(5), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(5), Index1:=igLineEnd, Object2:=objLines(6), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(6), Index1:=igLineEnd, Object2:=objLines(7), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(7), Index1:=igLineEnd, Object2:=objLines(8), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(8), Index1:=igLineEnd, Object2:=objLines(9), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(9), Index1:=igLineEnd, Object2:=objLines(10), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(10), Index1:=igLineEnd, Object2:=objLines(11), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(11), Index1:=igLineEnd, Object2:=objLines(12), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(12), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Check for Profile validity
    lngStatus = objProfile(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'Create the Base Extruded Protrusion Feature
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                             ProfileArray:=objProfile, ProfilePlaneSide:= _
                                                             igRight, ExtrusionDistance:=0.1)
    objProfile(1).Visible = False
    ' Check the status of Base Feature
    If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of Base Protrusion Feature object")
    End If

    '***** Create a Cutout object with 2 closed profiles
    '***** ProfileSide set to igLeft and ProfilePlaneSide set to igRight
    ' Create a Circular Profile
    Set objRefPln = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(2), _
                                                           Distance:=0.05, NormalSide:=igRight)
    Set objProf = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRefPln)
    Call objProf.Circles2d.AddByCenterRadius(x:=-0.02, y:=0.05, Radius:=0.005)
    Set objLines1 = objProf.Lines2d
    Call objLines1.AddBy2Points(x1:=-0.015, y1:=0.015, x2:=-0.015, y2:=0.02)
    Call objLines1.AddBy2Points(x1:=-0.015, y1:=0.02, x2:=-0.02, y2:=0.02)
    Call objLines1.AddBy2Points(x1:=-0.02, y1:=0.02, x2:=-0.02, y2:=0.015)
    Call objLines1.AddBy2Points(x1:=-0.02, y1:=0.015, x2:=-0.015, y2:=0.015)
    ' Define Relations among the Line objects to make the Profile closed
    Set objRelns1 = objProf.Relations2d
    Call objRelns1.AddKeypoint(Object1:=objLines1(1), Index1:=igLineEnd, Object2:=objLines1(2), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines1(2), Index1:=igLineEnd, Object2:=objLines1(3), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines1(3), Index1:=igLineEnd, Object2:=objLines1(4), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines1(4), Index1:=igLineEnd, Object2:=objLines1(1), Index2:=igLineStart)
    ' Check if the Profile is closed
    lngStatus = objProf.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'get profiles collection into an array
    Set objProfCollection = objProf.Parent.Profiles
    For i = 1 To objProfCollection.Count
        Set objProfArray(i) = objProfCollection(i)
        objProfArray(i).Visible = False
    Next i
    'Create the ExtrudedCutout feature
    Set objExtCut = objModel.ExtrudedCutouts.AddFiniteMulti _
                    (NumberOfProfiles:=2, ProfileArray:=objProfArray, _
                     ProfilePlaneSide:=igRight, Depth:=0.03)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProf = Nothing
    Set objProfile(1) = Nothing
    Set objProfile(2) = Nothing
    Set objExtCut = Nothing
    Set objModel = Nothing
    Set objLines = Nothing
    Set objLines1 = Nothing
    Set objRelns = Nothing
    Set objRelns1 = Nothing
    Set objRefPln = Nothing
    Set objProfCollection = Nothing
    Set objProfArray(1) = Nothing
    Set objProfArray(2) = Nothing
End Sub
See Also

ExtrudedCutouts Collection  | ExtrudedCutouts Members

Send comments on this topic.