Solid Edge Part Type Library
AttributeSets Property
Description
Returns the AttributeSets collection object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property AttributeSets As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProf As SolidEdgePart.Profile
    Dim objProfile(1 To 2) As SolidEdgePart.Profile
    Dim objExtCut As SolidEdgePart.ExtrudedCutout
    Dim objModel As SolidEdgePart.Model
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLines1 As SolidEdgeFrameworkSupport.Lines2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
    Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
    Dim objRefPln As SolidEdgePart.RefPlane
    Dim objProfCollection As SolidEdgePart.Profiles
    Dim objProfArray(1 To 2) As SolidEdgePart.Profile
    Dim objAttributeSets As Object
    Dim lngStatus As Long
    Dim i As Integer
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Draw the Base Profile
    Set objProfile(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(3))
    Set objLines = objProfile(1).Lines2d
    Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.08, y2:=0)
    Call objLines.AddBy2Points(x1:=0.08, y1:=0, x2:=0.08, y2:=0.08)
    Call objLines.AddBy2Points(x1:=0.08, y1:=0.08, x2:=0, y2:=0.08)
    Call objLines.AddBy2Points(x1:=0, y1:=0.08, x2:=0, y2:=0)
    ' Define Relations among the Line objects to make the Profile closed
    Set objRelns = objProfile(1).Relations2d
    Call objRelns.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Check for Profile validity
    lngStatus = objProfile(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'Create the Base Extruded Protrusion Feature
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                             ProfileArray:=objProfile, ProfilePlaneSide:= _
                                                             igRight, ExtrusionDistance:=0.1)
    objProfile(1).Visible = False
    ' Check the status of Base Feature
    If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of Base Protrusion Feature object")
    End If

    '***** Create a Cutout object with 2 closed profiles
    '***** ProfileSide set to igLeft and ProfilePlaneSide set to igRight
    ' Create a Circular Profile
    Set objRefPln = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(2), _
                                                           Distance:=0.05, NormalSide:=igRight)
    Set objProf = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRefPln)
    Call objProf.Circles2d.AddByCenterRadius(x:=-0.02, y:=0.05, Radius:=0.005)
    Set objLines1 = objProf.Lines2d
    Call objLines1.AddBy2Points(x1:=-0.015, y1:=0.015, x2:=-0.015, y2:=0.02)
    Call objLines1.AddBy2Points(x1:=-0.015, y1:=0.02, x2:=-0.02, y2:=0.02)
    Call objLines1.AddBy2Points(x1:=-0.02, y1:=0.02, x2:=-0.02, y2:=0.015)
    Call objLines1.AddBy2Points(x1:=-0.02, y1:=0.015, x2:=-0.015, y2:=0.015)
    ' Define Relations among the Line objects to make the Profile closed
    Set objRelns1 = objProf.Relations2d
    Call objRelns1.AddKeypoint(Object1:=objLines1(1), Index1:=igLineEnd, Object2:=objLines1(2), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines1(2), Index1:=igLineEnd, Object2:=objLines1(3), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines1(3), Index1:=igLineEnd, Object2:=objLines1(4), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines1(4), Index1:=igLineEnd, Object2:=objLines1(1), Index2:=igLineStart)
    ' Check if the Profile is closed
    lngStatus = objProf.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'get profiles collection into an array
    Set objProfCollection = objProf.Parent.Profiles
    For i = 1 To objProfCollection.Count
        Set objProfArray(i) = objProfCollection(i)
    Next i
    'Create the ExtrudedCutout feature
    Set objExtCut = objModel.ExtrudedCutouts.AddFiniteMulti _
                    (NumberOfProfiles:=2, ProfileArray:=objProfArray, _
                     ProfilePlaneSide:=igRight, Depth:=0.1)
    objProf.Visible = False
    If objExtCut.Status <> igFeatureOK Then
        MsgBox ("AddFiniteMulti Method with ProfileSide set to igLeft and ProfilePlaneSide set to igRight failed")
    End If
    'Attributesets
    Set objAttributeSets = objExtCut.AttributeSets
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProf = Nothing
    Set objProfile(1) = Nothing
    Set objProfile(2) = Nothing
    Set objExtCut = Nothing
    Set objModel = Nothing
    Set objLines = Nothing
    Set objLines1 = Nothing
    Set objRelns = Nothing
    Set objRelns1 = Nothing
    Set objRefPln = Nothing
    Set objProfCollection = Nothing
    Set objProfArray(1) = Nothing
    Set objProfArray(2) = Nothing
    Set objAttributeSets = Nothing
End Sub
See Also

ExtrudedCutout Object  | ExtrudedCutout Members

Send comments on this topic.