|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Description |  | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  DocumentName | Sets and returns the name of the full-path specification of the PartDocument name that contains the referenced DividedPart or FamilyMember object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  LiveRule | Turns a live rule on or off. | 
|  MovePrecedence | Controls the move precedence. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Status | Returns the status of the specified object. | 
|  SuppressedFeature | Returns the suppressed feature having a specified index of a part in a family. | 
|  SuppressedFeatureCount | Returns the number of suppressed features in a family of parts. | 
|  SuppressedRelationship | Returns the suppressed relationship having a specified index in a family. | 
|  SuppressedRelationshipCount | Returns the number of suppressed relationships in a family of parts. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  Value | Returns the name of the application, the value of a dimension, the value of a custom property, or the value of a variable. | 
|  Variable | Returns a Variable object having a specified index for the referenced FamilyMember object. | 
|  VariableCount | Returns the number of variables in a FamilyMember object. |