| Solid Edge Part Type Library : FlangeFeatureConstants Enumeration |
| Member | Value | Description |
|---|---|---|
| seFlangeBendAndFaceChainRelief | 3 | Corner Relief Extending Over The Chain of Adjacent Faces |
| seFlangeBendAndFaceCornerRelief | 2 | Corner Relief Over The Adjacent Bend And Face |
| seFlangeBendOnlyCornerRelief | 1 | Corner Relief Restricted To The Adjacent Bend Only |
| seFlangeBendOutside | 6 | Flange Placement Option - Bend Outside |
| seFlangeBendReliefNone | 9 | The Bend Relief Type - None |
| seFlangeBendReliefRound | 8 | The Bend Relief Type - Round |
| seFlangeBendReliefSquare | 7 | The Bend Relief Type - Square or Rectangular |
| seFlangeCornerReliefNone | 10 | The Corner Relief Type - None |
| seFlangeMaterialInside | 4 | Flange Placement Option - Material Inside |
| seFlangeMaterialOutside | 5 | Flange Placement Option - Material Outside |