Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BendAngle | |
BendRadius | Sets and returns the inside radius of the bend. |
BendReliefDepth | Sets and returns the depth of the bend relief for the specified object. |
BendReliefType | Sets and returns a constant that specifies the Bend relief type. |
BendReliefWidth | Sets and returns the width of the bend relief for the specified object. |
ConstructionEdge | Returns the ConstructionEdge object for the referenced Flange object. |
CornerReliefType | Property That Specifies The Corner Relief Type To Be Used |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FlangeMaterialSide | Specifies the flange location. |
HotEdge | Returns the HotEdge object for the referenced Flange object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | |
Name | Returns the name of the referenced object. |
NeutralFactor | Sets and returns the neutral factor applied to the bend. |
OffsetType | |
OffsetValue | This read-write Double property sets and returns the offset value for the referenced Flange object. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
UseGlobalBendRadius | Specifies whether or not the global bend radius is to be applied to the referenced object. |
UseGlobalBendReliefDepth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. |
UseGlobalBendReliefWidth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. |
UseGlobalNeutralFactor | Specifies whether or not the global neutral factor is to be applied to the referenced object. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |