Solid Edge Part Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Name As String
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBaseProfile As SolidEdgePart.Profile
    Dim objBaseProfileArray(1 To 2) As SolidEdgePart.Profile
    Dim objBaseModel As SolidEdgePart.Model
    Dim objProfile As SolidEdgePart.Profile
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objRefAxis As SolidEdgePart.RefAxis
    Dim objCrossSection As SolidEdgeFrameworkSupport.Circle2d
    Dim objCSArray(1 To 2) As SolidEdgePart.Profile
    Dim objHelixCutout As SolidEdgePart.HelixCutout
    Dim lngStatus As Long
    Dim sName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** creating the base feature
    ' creating a circular profile and validating it
    Set objBaseProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objBaseProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.05)
    lngStatus = objBaseProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the Base feature is not closed"
        Exit Sub
    End If
    Set objBaseProfileArray(1) = objBaseProfile
    ' creating the base feature
    Set objBaseModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                                 ProfileArray:=objBaseProfileArray, ProfilePlaneSide:=igSymmetric, ExtrusionDistance:=0.1)
    objBaseProfile.Visible = False
    ' *** creating a helix cutout feature
    ' creating a circular profile and a reference axis and validating it
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Set objLine = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=0.05, x2:=0, y2:=-0.05)
    Set objRefAxis = objProfile.SetAxisOfRevolution(LineForAxis:=objLine)
    Set objCrossSection = objProfile.Circles2d.AddByCenterRadius(x:=0.025, y:=-0.05, Radius:=0.01)
    lngStatus = objProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the helix cutout feature is not closed"
        Exit Sub
    End If
    Set objCSArray(1) = objProfile
    ' creating the helix cutout feature and validating it
    Set objHelixCutout = objDoc.Models(1).HelixCutouts.AddFinite(HelixAxis:=objRefAxis, _
                                                                 AxisStart:=igEnd, NumCrossSections:=1, CrossSectionArray:=objCSArray, _
                                                                 ProfileSide:=igRight, Height:=0.1, Pitch:=0.025, NumberOfTurns:=4, HelixDir:=igRight)
    objProfile.Visible = False
    If (objHelixCutout.Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the HelixCutouts object fails"
    End If
    ' geting the name of the helix cutout feature
    sName = objHelixCutout.Name
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBaseProfile = Nothing
    Set objBaseProfileArray(1) = Nothing
    Set objBaseModel = Nothing
    Set objProfile = Nothing
    Set objLine = Nothing
    Set objRefAxis = Nothing
    Set objCrossSection = Nothing
    Set objCSArray(1) = Nothing
    Set objHelixCutout = Nothing
End Sub
See Also

HelixCutout Object  | HelixCutout Members

Send comments on this topic.