Solid Edge Part Type Library
AttributeSets Property
Description
Returns the AttributeSets collection object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property AttributeSets As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objHoles As SolidEdgePart.Holes2d
    Dim objHole2d As SolidEdgePart.Hole2d
    Dim objProfile As SolidEdgePart.Profile
    Dim objAttributeSets As Object
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Holes2d collection object
    Set objHoles = objProfile.Holes2d
    ' Create a Hole2d object
    Set objHole2d = objHoles.Add(xCenter:=0, yCenter:=0)
    ' Get the Attributesets collection object
    Set objAttributeSets = objHole2d.AttributeSets
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objHoles = Nothing
    Set objHole2d = Nothing
    Set objProfile = Nothing
    Set objAttributeSets = Nothing
End Sub
See Also

Hole2d Object  | Hole2d Members

Send comments on this topic.