Solid Edge Part Type Library
Duplicate Method
Specifies the distance in the x direction from the original that the copy of the referenced object is to be placed.
Specifies the distance in the y direction from the original that the copy of the referenced object is to be placed.
Description
Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original.
Syntax
Visual Basic
Public Function Duplicate( _
   Optional ByVal XDistance As Variant, _
   Optional ByVal YDistance As Variant _
) As Object
Parameters
XDistance
Specifies the distance in the x direction from the original that the copy of the referenced object is to be placed.
YDistance
Specifies the distance in the y direction from the original that the copy of the referenced object is to be placed.
Remarks
The referenced object is copied to the new location relative to the original (source) location. The distance is the difference from the object's original location to the XDistance and YDistance values. The new object is returned.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objHols As SolidEdgePart.Holes2d
    Dim objHol2d As SolidEdgePart.Hole2d
    Dim objProfile As SolidEdgePart.Profile
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Holes2d collection object
    Set objHols = objProfile.Holes2d
    ' Create a Hole2d object
    Set objHol2d = objHols.Add(xCenter:=0, yCenter:=0)
    ' Make 3 Duplicates of the Hole2d object at specified distance
    Call objHol2d.Duplicate(xDistance:=0.1)
    Call objHol2d.Duplicate(yDistance:=0.1)
    Call objHol2d.Duplicate(xDistance:=0.1, yDistance:=0.1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objHols = Nothing
    Set objHol2d = Nothing
    Set objProfile = Nothing
End Sub
See Also

Hole2d Object  | Hole2d Members

Send comments on this topic.