Solid Edge Part Type Library
DraftAngle Property
Collapse All
Expand All
Solid Edge Part Type Library
>
Hole Object
: DraftAngle Property
Description
Sets and returns the angle at which the hole is angled from the normal of the reference plane.
Property type
Read-write property
Syntax
Visual Basic
Public Property DraftAngle As Double
See Also
Hole Object
|
Hole Members
Send comments
on this topic.