Solid Edge Part Type Library
Add Method
Specifies the AsmSource object on which the InterpartConstruction object is to be based.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal AsmSource As Object _
) As InterpartConstruction
Parameters
AsmSource
Specifies the AsmSource object on which the InterpartConstruction object is to be based.
See Also

InterpartConstructions Collection  | InterpartConstructions Members

Send comments on this topic.