|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BendParamType | Sets and returns the method to be used when specifying the bend neutral factor. | 
|  BendRadius | Sets and returns the inside radius of the bend. | 
|  BendReliefDepth | Sets and returns the depth of the bend relief for the specified object. | 
|  BendReliefType | Sets and returns a constant that specifies the Bend relief type. | 
|  BendReliefWidth | Sets and returns the width of the bend relief for the specified object. | 
|  CornerReliefType | Sets and returns a constant that specifies the corner relief type. | 
|  DimensionType | Sets and returns the type of dimension for the referenced object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  ExtendBendRelief |  | 
|  ExtendMoldLines | Sets and returns a constant that specifies whether or not to extend mold lines. | 
|  Extent | Sets and returns the extent of the referenced object. | 
|  ExtentType | Sets and returns the extent type for the referenced object. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  JogDirection | Sets and returns the direction for the referenced Jog object. | 
|  MaterialSide | Sets and returns the direction in which material was added to the referenced object. | 
|  MovingSide | Sets and returns a constant that specifies the side of the base part, with respect to the profile, that will move to become the created face. | 
|  Name | Returns the name of the referenced object. | 
|  NeutralFactor | Sets and returns the neutral factor applied to the bend. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Profile | Sets and returns the Profile object used to construct the referenced feature object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  UseGlobalBendRadius | Specifies whether or not the global bend radius is to be applied to the referenced object. | 
|  UseGlobalBendReliefDepth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. | 
|  UseGlobalBendReliefWidth | Specifies whether or not the global bend relief width is to be applied to the referenced object. | 
|  UseGlobalNeutralFactor | Specifies whether or not the global neutral factor is to be applied to the referenced object. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |