Solid Edge Part Type Library
EndpointMagnitude Property
Collapse All
Expand All
Solid Edge Part Type Library
>
KeyPointCurve Object
: EndpointMagnitude Property
Description
Sets and returns the direction and degree of influence of the EndpointEdge on the curvature of the curve at the endpoint.
Property type
Read-write property
Syntax
Visual Basic
Public Property EndpointMagnitude As Double
Remarks
This value is meaningful only if the EndpointEndCondition is seKeypointEndConditionTangent.
See Also
KeyPointCurve Object
|
KeyPointCurve Members
Send comments
on this topic.