Solid Edge Part Type Library
StartpointMagnitude Property
Collapse All
Expand All
Solid Edge Part Type Library
>
KeyPointCurve Object
: StartpointMagnitude Property
Description
Sets and returns the direction and degree of influence of the StartpointEdge on the curvature of the curve at the startpoint.
Property type
Read-write property
Syntax
Visual Basic
Public Property StartpointMagnitude As Double
Remarks
This value is meaningful only if the StartpointEndCondition is seKeypointEndConditionTangent.
See Also
KeyPointCurve Object
|
KeyPointCurve Members
Send comments
on this topic.