Solid Edge Part Type Library
Edges Property
Description
Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Property type
Read-only property
Syntax
Visual Basic
Public Property Edges( _
   ByVal EdgeType As FeatureTopologyQueryTypeConstants _
) As Object
Parameters
EdgeType
ValueDescription
igQueryAllFeature Topology Query Type - All
igQueryConeFeature Topology Query Type - Cone
igQueryCylinderFeature Topology Query Type - Cylinder
igQueryEllipseFeature Topology Query Type - Ellipse
igQueryPlaneFeature Topology Query Type - Plane
igQueryRoundableFeature Topology Query Type - Roundable
igQuerySphereFeature Topology Query Type - Sphere
igQuerySplineFeature Topology Query Type - Spline
igQueryStraightFeature Topology Query Type - Straight
igQueryTorusFeature Topology Query Type - Torus
Remarks
The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. By default, the Edges property returns all edges for the object. The topology collection can be restricted to a specified type of edge by supplying a value (from the FeatureTopologyQueryTypeConstants constant set) for the EdgeType argument for the feature objects only. For example, this property can be set to return all ellipse edges, straight edges, and so forth.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objProfArr(1 To 2) As SolidEdgePart.Profile
    Dim objModel As SolidEdgePart.Model
    Dim objExtProt As SolidEdgePart.ExtrudedProtrusion
    Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
    Dim objEdges(1 To 1) As Object
    Dim objSideFace As Object
    Dim objCapFace As Object
    Dim objLips As SolidEdgePart.Lips
    Dim objLip As SolidEdgePart.Lip
    Dim objLipEdges As Object
    Dim lngStatus As Long
    Dim i As Integer
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Draw the Profile
    Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Set objLines = objProfArr(1).Lines2d
    Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.06, y2:=0)
    Call objLines.AddBy2Points(x1:=0.06, y1:=0, x2:=0.06, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.06, y1:=0.06, x2:=0, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0, y1:=0.06, x2:=0, y2:=0)
    ' Relate the Lines to make the Profile closed
    Set objRelns1 = objProfArr(1).Relations2d
    Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Check for the Profile Validity
    lngStatus = objProfArr(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    ' Create the Base Protrusion Object
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                             ProfileArray:=objProfArr, profileplaneSide:=igRight, _
                                                             ExtrusionDistance:=0.02)
    objProfArr(1).Visible = False
    ' Check the status of Base Feature
    If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of Base Protrusion Feature object")
    End If
    Set objExtProt = objModel.ExtrudedProtrusions(1)
    '*** Lip Creation
    'Get the Lips collection from the Model object
    Set objLips = objModel.Lips
    'Get the edges on which lip is to be created in to an array
    Set objEdges(1) = objExtProt.BottomCap.Edges.Item(1)
    'Get the face to be set as SideFace for the Lip
    Set objSideFace = objExtProt.SideFaces.Item(1)
    'Get the face to be set as CapFace for the Lip
    Set objCapFace = objExtProt.BottomCap
    'Create the Lip
    Set objLip = objLips.Add(Numberofedges:=1, Edges:=objEdges, SideFace:=objSideFace, _
                             CapFace:=objCapFace, Width:=0.01, Height:=0.005)
    'Validate the feature
    If objLip.Status <> igFeatureOK Then
        MsgBox "Add method of Lip feature failed"
    End If
    'Get the Edges collection of Lip object
    Set objLipEdges = objLip.Edges(edgetype:=igQueryAll)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objProfArr(1) = Nothing
    Set objProfArr(2) = Nothing
    Set objModel = Nothing
    Set objExtProt = Nothing
    Set objRelns1 = Nothing
    Set objEdges(1) = Nothing
    Set objSideFace = Nothing
    Set objCapFace = Nothing
    Set objLips = Nothing
    Set objLip = Nothing
    Set objLipEdges = Nothing
End Sub
See Also

Lip Object  | Lip Members

Send comments on this topic.