| Solid Edge Part Type Library : LiveRulesConstants Enumeration |
| Member | Value | Description |
|---|---|---|
| igConcentricLiveRule | 1 | Maintain concentric relations |
| igCoplanarAxesAboutXLiveRule | 14 | |
| igCoplanarAxesAboutYLiveRule | 15 | |
| igCoplanarAxesAboutZLiveRule | 16 | |
| igCoplanarAxesLiveRule | 13 | Maintain coplanar Axes. Always on for live rules in an FOP and cannot be turned off. |
| igCoplanarLiveRule | 2 | Maintain coplanar relations |
| igMaintainRadiusLiveRule | 11 | Maintain same radius if possible |
| igOrthoLockingLiveRule | 12 | Maintain orthogonal to base if possible |
| igParallelLiveRule | 5 | Maintain parallel relations |
| igPerpendicularLiveRule | 6 | Maintain perpendicular relations |
| igSymmetricLiveRule | 7 | Maintain symmetric relations |
| igSymmetricXYLiveRule | 8 | Maintain symmetric relations based on XY plane |
| igSymmetricYZLiveRule | 9 | Maintain symmetric relations based on YZ plane |
| igSymmetricZXLiveRule | 10 | Maintain symmetric relations based on ZX plane |
| igTangentEdgeLiveRule | 3 | Maintain connected tangent relations |
| igTangentTouchingLiveRule | 4 | Maintain touching tangent relations |
| igThicknessChainLiveRule | 17 |