| Solid Edge Part Type Library : LiveSection Object |
Delete | Deletes the referenced object. |
Range | Returns the high and low range values for the referenced object. |
Application | Returns the active application object. |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Status | Returns the status of the specified object. |
SystemName | |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |