Solid Edge Part Type Library
AddLoad Method
Geometries
Load Type
Load Value
Ang Accn Load Value
For force direction
X Direction
Y Direction
Z Direction
X Direction
Y Direction
Z Direction
Color of the load symbols
Color of the symbols
Symbol spacing factor
Symbol size factor
Steering wheel length
Load properties
Load symbol spacing factor
Load symbol size
Description
Create a new load object.
Syntax
Visual Basic
Public Sub AddLoad( _
   ByRef arrStudyGeomeProxies() As Object, _
   ByVal eLoadType As FEALoadTypeEnum_Auto, _
   ByVal dLoadValue As Double, _
   ByVal dLoadValueAngAcceln As Double, _
   ByVal eLoadDir As LoadSymbDirOptsEnum_Auto, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double, _
   ByVal xx As Double, _
   ByVal yy As Double, _
   ByVal zz As Double, _
   ByVal colorLoadSymbol As ULong, _
   ByVal colorLoadSymbolAngAcc As ULong, _
   ByVal dSpacingFactor As Double, _
   ByVal dSizeFactor As Double, _
   ByVal dSteeringWheelLen As Double, _
   ByVal dwLoadProps As ULong, _
   ByVal dLoadSymSpacing As Double, _
   ByVal dLoadSymSize As Double, _
   ByRef ppLoad As Object _
) 
Parameters
arrStudyGeomeProxies
Geometries
eLoadType
ValueDescription
eLoadTypeBearing_Auto 
eLoadTypeCentrifugal_Auto 
eLoadTypeEnforcedDisplacement_Auto 
eLoadTypeEnforcedRotation_Auto 
eLoadTypeForce_Auto 
eLoadTypeGravity_Auto 
eLoadTypeMoment_Auto 
eLoadTypeNone_Auto 
eLoadTypePressure_Auto 
eLoadTypeSSHTConvection_Auto 
eLoadTypeSSHTHeatflux_Auto 
eLoadTypeSSHTHeatGeneration_Auto 
eLoadTypeSSHTRadiation_Auto 
eLoadTypeSSHTTemperature_Auto 
eLoadTypeTemperature_Auto 
eLoadTypeTorque_Auto 
Load Type
dLoadValue
Load Value
dLoadValueAngAcceln
Ang Accn Load Value
eLoadDir
ValueDescription
eLoadDirAboutAxis_Auto 
eLoadDirAlongVec_Auto 
eLoadDirCentrifugal_Auto 
eLoadDirComponents_Auto 
eLoadDirDefault_Auto 
eLoadDirForCnstr_Auto 
eLoadDirGravity_Auto 
eLoadDirHeatFlux_Auto 
eLoadDirNormalToFace_Auto 
eLoadDirTorque_Auto 
For force direction
x
X Direction
y
Y Direction
z
Z Direction
xx
X Direction
yy
Y Direction
zz
Z Direction
colorLoadSymbol
Color of the load symbols
colorLoadSymbolAngAcc
Color of the symbols
dSpacingFactor
Symbol spacing factor
dSizeFactor
Symbol size factor
dSteeringWheelLen
Steering wheel length
dwLoadProps
Load properties
dLoadSymSpacing
Load symbol spacing factor
dLoadSymSize
Load symbol size
ppLoad
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objLoadOwner As SolidEdgePart.LoadOwner = Nothing
        Dim objLoad As SolidEdgePart.Load = Nothing
        Dim objProxiesArray(1) As Object
        Dim eLoadDirection As SolidEdgePart.LoadSymbDirOptsEnum_Auto
        Dim eLoadType As SolidEdgePart.FEALoadTypeEnum_Auto
        Dim dLoadValue As Double = 2500000
        Dim dLoadDirX As Double = -0.0
        Dim dLoadDirY As Double = 1.0
        Dim dLoadDirZ As Double = -0.0
        Dim dLoadPosX As Double = -0.0754203151729549
        Dim dLoadPosY As Double = 0.015441908335819984
        Dim dLoadPosZ As Double = 0.056796356131827666
        Dim dSpacingFactor As Double = 0.11
        Dim dSizeFactor As Double = 0.24200000000000002
        Dim dSteeringWheelLen As Double = 0.020253310860972911
        Dim dwLoadProps As UInt32 = 0
        Dim dLoadSymSpacing As Double = 0.016464634271235477
        Dim dLoadSymSize As Double = 0.036222195396718053
        Dim ColorLoadSymbol As UInt32 = 16736256
        Dim ColorLoadSymbolAngAcc As UInt32 = 8388673

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudy = objStudyOwner.Item(1)
            objStudy.GetLoadOwner(objLoadOwner)

            eLoadDirection = SolidEdgePart.LoadSymbDirOptsEnum_Auto.eLoadDirForCnstr_Auto
            eLoadType = SolidEdgePart.FEALoadTypeEnum_Auto.eLoadTypeForce_Auto

            ' Populate objProxiesArray

            objLoadOwner.AddLoad(objProxiesArray, _
                                 eLoadType, _
                                 dLoadValue, _
                                 0, _
                                 eLoadDirection, _
                                 dLoadDirX, _
                                 dLoadDirY, _
                                 dLoadDirZ, _
                                 dLoadPosX, _
                                 dLoadPosY, _
                                 dLoadPosZ, _
                                 ColorLoadSymbol, _
                                 ColorLoadSymbolAngAcc, _
                                 dSpacingFactor, _
                                 dSizeFactor, _
                                 dSteeringWheelLen, _
                                 dwLoadProps, _
                                 dLoadSymSpacing, _
                                 dLoadSymSize, _
                                 objLoad)
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

LoadOwner Object  | LoadOwner Members  | Solid Edge ST3 - What's New

Send comments on this topic.