Public Methods
Delete | Delete a perticular load object. |
GetFlip | Ger current Flip condition of load. |
GetGeometries | Get an array of geometry objects on which the load has been applied. |
GetLoadDirection | Get X, Y, Z directions from a load object. |
GetLoadOptions | Get various option parameter values from existing load. |
GetLoadType | Get type of a load object. |
GetLoadValue | Get value of a load object. |
GetLoadValueAngAcceln | Get value of angular acceleration load object. |
GetThermalLoadOptions | Get various option parameter values from existing Thermal load. |
SetFlip | Flip load direction, towards/away from entity. |
SetGeometries | Set edges/faces/vertices etc as geometry to apply load on. |
SetLoadDirection | Set X, Y, Z directions for a load object. |
SetLoadOptions | Set/modify parameters like load value, symbol spacing, symbol size of an existing load object. |
SetLoadType | Set type of a load object. |
SetLoadValue | Set value on a load object. |
SetLoadValueAngAcceln | Set value of angular acceleration load object. |
SetThermalLoadOptions | Set/modify parameters like load value, symbol spacing, symbol size, ambient temperature, view factor etc of an existing Thermal load object. |
See Also