Solid Edge Part Type Library
Add Method
Required Doubles that specify the center of the profile.
Required Doubles that specify the center of the profile.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal XCenter As Double, _
   ByVal YCenter As Double _
) As MountingBoss2d
Parameters
XCenter
Required Doubles that specify the center of the profile.
YCenter
Required Doubles that specify the center of the profile.
See Also

MountingBoss2dCollection Collection  | MountingBoss2dCollection Members

Send comments on this topic.