|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BossDiameter | Specifies the diameter of the referenced MountingBoss object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  DraftAngle | Specifies the draft angle. | 
|  DraftEnabled | Specifies whether draft is enabled. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelingModeType | Returns the modeling mode of the referenced object. | 
|  MountingHoleDepth | Specifies the depth of the mounting hole. | 
|  MountingHoleDiameter | Specifies the diameter of the mounting hole. | 
|  MountingHoleEnabled | Specifies whether mounting hole is enabled for the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  NumberInputFeatures | Returns the number of input features for the referenced feature. | 
|  NumberOfRibs | Specifies the number of ribs. | 
|  OccurrenceIndex | Returns the index for the feature occurrence for the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PatternPlane | Returns the PatternPlane for the referenced object. | 
|  ProfilePlaneSide | Specifies the profile plane side for the referenced object. | 
|  RibExtent | Specifies the distance the ribs protrude from the side of the referenced object. | 
|  RibGrade | Specifies the angle of the ribs relative to the top face of the referenced MountingBoss object. | 
|  RibOffset | Specifies the distance the ribs are offset from the top surface. | 
|  RibsEnabled | Specifies whether ribs are enabled. | 
|  RibTaper | Specifies the angle of the ribs relative to the cylindrical body. | 
|  RibThickness | Specifies the thickness of the ribs. | 
|  RoundEnabled | Specifies whether rounding is enabled. | 
|  RoundRadius | Specifies the radius of the round. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Transforms | Returns a read-only variant. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |