Solid Edge Part Type Library
LongestCurveSide Property
Description
Sets or gets the side of the longest curve, with reference to which to the protrusion is placed
Property type
Read-write property
Syntax
Visual Basic
Public Property LongestCurveSide As FeaturePropertyConstants
See Also

NormalToFaceProtrusion Object  | NormalToFaceProtrusion Members

Send comments on this topic.