Solid Edge Part Type Library
Add Method
Specifies the Profile object on which the PatternPart feature is based.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal Profile As Profile _
) As PatternPart
Parameters
Profile
Specifies the Profile object on which the PatternPart feature is based.
See Also

PatternParts Collection  | PatternParts Members

Send comments on this topic.