| Solid Edge Part Type Library : Plot Object |
GetMaxNodeOnBody | Gets the node with maximum value on the given body. |
GetMaxNodeOnSurface | Gets the node with maximum value on the given surface. |
GetMinMaxValues | Get minimun and maximum stress/displacement values. |
GetMinNodeOnBody | Gets the node with minimum value on the given body. |
GetMinNodeOnSurface | Gets the node with minimum value on the given surface. |
GetNearestNode | Returns the data on the node nearest to xyz. In the case of a tie, the first node found should be used. |
GetNodesOnFace | Returns all the Nodes on a given face as an array or list |
GetPlotType | Get plot object type. |
GetXYZLocationsOfMaxValue | Get maximum values at X, Y and Z locations. |
GetXYZLocationsOfMinValue | Get minimum values at X, Y and Z locations. |
SavePlotAsImage | Save plot display as an image to given location. |
SavePlotAsMovie | Save plot animation as a movie to given location. |