Solid Edge Part Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfileSets As SolidEdgePart.ProfileSets
    Dim objParent As SolidEdgePart.PartDocument
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create the ProfileSets object
    Set objProfileSets = objDoc.ProfileSets
    ' Get the Parent property
    Set objParent = objProfileSets.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfileSets = Nothing
    Set objParent = Nothing
End Sub
See Also

ProfileSets Collection  | ProfileSets Members

Send comments on this topic.