Solid Edge Part Type Library
Delete Method
Description
Deletes the referenced object.
Syntax
Visual Basic
Public Sub Delete() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfileSet As SolidEdgePart.ProfileSet
    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Create a ProfileSet object
    Set objProfileSet = objDoc.ProfileSets.Add
    'Delete the ProfileSet object
    Call objProfileSet.Delete
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfileSet = Nothing
End Sub
See Also

ProfileSet Object  | ProfileSet Members

Send comments on this topic.