Solid Edge Part Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfiles As SolidEdgePart.Profiles
    Dim objApplicn As SolidEdgeFramework.Application
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a Profiles collection object
    Set objProfiles = objDoc.ProfileSets.Add.Profiles
    ' Get the Application property
    Set objApplicn = objProfiles.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfiles = Nothing
    Set objApplicn = Nothing
End Sub
See Also

Profiles Collection  | Profiles Members

Send comments on this topic.