Solid Edge Part Type Library
FaceMergeOption Property
Description
Get set property for deciding which option to be used for Face merging.
Property type
Read-write property
Syntax
Visual Basic
Public Property FaceMergeOption As SurfaceByBoundaryPatchTopology
Example
Following options are available.
igSurfaceByBoundaryMinimal – Merge (as many as possible)
igSurfaceByBoundaryMultiple – No Merge
igSurfaceByBoundarySingle – Full Merge
See Also

RedefineFace Object  | RedefineFace Members

Send comments on this topic.