Solid Edge Part Type Library
GetEdgeTangencyTypes Method
Number of edges.
Array of boundary edges.
Description
Get the edges input for redefine surface and its corresponding tangency types.
Syntax
Visual Basic
Public Sub GetEdgeTangencyTypes( _
   ByRef NumberOfEdgesAndTypes As Long, _
   ByRef BoundaryEdgesArray() As Object, _
   ByRef TangencyTypeArray() As RedefineFaceTangencyType _
) 
Parameters
NumberOfEdgesAndTypes
Number of edges.
BoundaryEdgesArray
Array of boundary edges.
TangencyTypeArray
ValueDescription
igRedefineFaceCurvatureContinuous
igRedefineFaceNatural
igRedefineFaceNormalToPlane
igRedefineFaceTangentContinuous
Remarks
Tangency types could be one of the following:
-igNatural
-igTangent
-igCurvatureContinous
-igNormal (only for sketch edges created by redefine surface)
See Also

RedefineFace Object  | RedefineFace Members

Send comments on this topic.