Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objRefAxis As SolidEdgePart.RefAxis
    Dim objRefAxis1 As SolidEdgePart.RefAxis
    Dim lngStatus As Long
    Dim strName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a Profile object
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(3))
    'Create a Line Object
    Set objLine = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
    ' Check the validation criteria of the profile
    lngStatus = objProfile.End(ValidationCriteria:=igProfileSingle)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the reference axis is not open"
    End If
    ' Create a reference axis using the line.
    Set objRefAxis = objProfile.SetAxisOfRevolution(lineforaxis:=objLine)
    'Create a RefAxis object
    Set objRefAxis1 = objDoc.RefAxes(1)
    ' Get the name of the RefAxis object
    strName = objRefAxis1.Name
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objLine = Nothing
    Set objRefAxis = Nothing
    Set objRefAxis1 = Nothing
End Sub