Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objRefAxis As SolidEdgePart.RefAxis
    Dim objModel As SolidEdgePart.Model
    Dim objProfileArray(1 To 2) As SolidEdgePart.Profile
    Dim objRevCutout As SolidEdgePart.RevolvedCutout
    Dim objCutoutProfile As SolidEdgePart.Profile
    Dim objCutoutLine As SolidEdgeFrameworkSupport.Line2d
    Dim objCutoutRefAxis As SolidEdgePart.RefAxis
    Dim objTCRefPlane As SolidEdgePart.RefPlane
    Dim objTCProfile As SolidEdgePart.Profile
    Dim objTCRefAxis As SolidEdgePart.RefAxis
    Dim objTCRevProt As SolidEdgePart.RevolvedProtrusion
    Dim objTCLine As SolidEdgeFrameworkSupport.Line2d
    Dim objBCRefPlane As SolidEdgePart.RefPlane
    Dim objBCProfile As SolidEdgePart.Profile
    Dim objBCRefAxis As SolidEdgePart.RefAxis
    Dim objBCRevProt As SolidEdgePart.RevolvedProtrusion
    Dim objBCLine As SolidEdgeFrameworkSupport.Line2d
    Dim dblAngle As Double
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** creating the Base Feature (Revolved Protrusion)
    ' creating the cross-section profile and the reference axis for the base feature
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Call objProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0, Radius:=0.025)
    lngStatus = objProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the base feature is not closed"
    End If
    Set objLine = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
    Set objRefAxis = objProfile.SetAxisOfRevolution(LineForAxis:=objLine)
    ' creating the revolved protrusion feature and validating it
    Set objProfileArray(1) = objProfile.Parent.Profiles(1)
    Set objModel = objDoc.Models.AddFiniteRevolvedProtrusion(NumberOfProfiles:=1, ProfileArray:=objProfileArray, _
                                                             ReferenceAxis:=objRefAxis, ProfilePlaneSide:=igSymmetric, AngleOfRevolution:=(PI))
    objProfileArray(1).Visible = False
    If (objModel.RevolvedProtrusions(1).Status <> igFeatureOK) Then
        MsgBox "AddFiniteRevolvedProtrusion method of the Models object fails"
    End If
    ' *** creating a revolved protrusion on the base feature
    ' creating a circular profile on the topcap of the base feature
    Set objTCRefPlane = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objModel.RevolvedProtrusions(1).TopCap, _
                                                               Distance:=0, NormalSide:=igRight, Local:=True)
    Set objTCProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objTCRefPlane)
    Call objTCProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.02)
    lngStatus = objTCProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "profile for the revolved protrusion on top cap feature is not closed"
    End If
    Set objTCLine = objTCProfile.Lines2d.AddBy2Points(x1:=0.05, y1:=-0.05, x2:=0.05, y2:=0.05)
    Set objTCRefAxis = objTCProfile.SetAxisOfRevolution(LineForAxis:=objTCLine)
    ' creating the revolved protrusion feature and validating it
    Set objTCRevProt = objModel.RevolvedProtrusions.AddFinite(Profile:=objTCProfile, _
                                                              RefAxis:=objTCRefAxis, profileSide:=igLeft, ProfilePlaneSide:=igRight, AngleOfRevolution:=(PI / 6))
    objTCProfile.Visible = False
    If (objModel.RevolvedProtrusions(2).Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the RevolvedProtrusions object fails"
    End If
    ' *** creating a revolved protrusion on the base feature
    ' creating a circular profile on the bottomcap of the base feature
    Set objBCRefPlane = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objModel.RevolvedProtrusions(1).BottomCap, _
                                                               Distance:=0, NormalSide:=igRight, Local:=True)
    Set objBCProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objBCRefPlane)
    Call objBCProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.02)
    lngStatus = objBCProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "profile for the revolved protrusion on bottom cap feature is not closed"
    End If
    Set objBCLine = objBCProfile.Lines2d.AddBy2Points(x1:=-0.05, y1:=-0.05, x2:=-0.05, y2:=0.05)
    Set objBCRefAxis = objBCProfile.SetAxisOfRevolution(LineForAxis:=objBCLine)
    ' creating the revolved protrusion feature and validating it
    Set objBCRevProt = objModel.RevolvedProtrusions.AddFinite(Profile:=objBCProfile, _
                                                              RefAxis:=objBCRefAxis, profileSide:=igLeft, ProfilePlaneSide:=igRight, AngleOfRevolution:=(PI / 6))
    objBCProfile.Visible = False
    If (objModel.RevolvedProtrusions(3).Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the RevolvedProtrusions object fails"
    End If
    ' *** creating a Revolved Cutout in the Base Feature
    ' creating the cross-section and the reference axis for the revolved cutout feature
    Set objCutoutProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Call objCutoutProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0, Radius:=0.01)
    lngStatus = objCutoutProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "profile for the revolved cutout feature is not closed"
    End If
    Set objCutoutLine = objCutoutProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
    Set objCutoutRefAxis = objCutoutProfile.SetAxisOfRevolution(LineForAxis:=objCutoutLine)
    ' creating the revolved cutout feature and validating it
    Set objRevCutout = objModel.RevolvedCutouts.AddFinite(Profile:=objCutoutProfile, _
                                                          RefAxis:=objCutoutRefAxis, profileSide:=igLeft, ProfilePlaneSide:=igSymmetric, AngleOfRevolution:=(3 * PI / 4))
    objCutoutProfile.Visible = False
    If (objModel.RevolvedCutouts(1).Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the RevolvedCutouts object fails"
    End If
    ' reordering the revolved cutout feature to place it after the revolved protrusion on bottomcap of base feature
    Call objRevCutout.Reorder(TargetFeature:=objTCRevProt, InsertBefore:=False)
    ' checking whether the revolved cutout feature has been properly reordered
    If Not (objModel.Features(3) Is objRevCutout) Then
        MsgBox "Reorder method failed to place the revolved cutout feature after the revolved protrusion feature"
    End If
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objLine = Nothing
    Set objRefAxis = Nothing
    Set objModel = Nothing
    Set objProfileArray(1) = Nothing
    Set objProfileArray(2) = Nothing
    Set objRevCutout = Nothing
    Set objCutoutProfile = Nothing
    Set objCutoutLine = Nothing
    Set objCutoutRefAxis = Nothing
    Set objTCRefPlane = Nothing
    Set objTCProfile = Nothing
    Set objTCRefAxis = Nothing
    Set objTCRevProt = Nothing
    Set objTCLine = Nothing
    Set objBCRefPlane = Nothing
    Set objBCProfile = Nothing
    Set objBCRefAxis = Nothing
    Set objBCRevProt = Nothing
    Set objBCLine = Nothing
End Sub