Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objRefAxis As SolidEdgePart.RefAxis
    Dim objModel As SolidEdgePart.Model
    Dim objProfileArray(1 To 2) As SolidEdgePart.Profile
    Dim objRevCutout As SolidEdgePart.RevolvedCutout
    Dim objCutoutProfile As SolidEdgePart.Profile
    Dim objCutoutLine As SolidEdgeFrameworkSupport.Line2d
    Dim objCutoutRefAxis As SolidEdgePart.RefAxis
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** creating the Base Feature (Revolved Protrusion)
    ' creating the cross-section profile and the reference axis for the base feature
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Call objProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0, Radius:=0.025)
    lngStatus = objProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the base feature is not closed"
    End If
    Set objLine = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
    Set objRefAxis = objProfile.SetAxisOfRevolution(LineForAxis:=objLine)
    ' creating the revolved protrusion feature and validating it
    Set objProfileArray(1) = objProfile.Parent.Profiles(1)
    Set objModel = objDoc.Models.AddFiniteRevolvedProtrusion(NumberOfProfiles:=1, ProfileArray:=objProfileArray, _
                                                             ReferenceAxis:=objRefAxis, ProfilePlaneSide:=igSymmetric, AngleOfRevolution:=(3 * PI / 2))
    objProfileArray(1).Visible = False
    If (objModel.RevolvedProtrusions(1).Status <> igFeatureOK) Then
        MsgBox "AddFiniteRevolvedProtrusion method of the Models object fails"
    End If
    ' *** creating a Revolved Cutout in the Base Feature towards right
    ' creating the cross-section and the reference axis for the revolved cutout feature
    Set objCutoutProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Call objCutoutProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0, Radius:=0.01)
    lngStatus = objCutoutProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "profile for the revolved cutout feature is not closed"
    End If
    Set objCutoutLine = objCutoutProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
    Set objCutoutRefAxis = objCutoutProfile.SetAxisOfRevolution(LineForAxis:=objCutoutLine)
    ' creating the revolved cutout feature and validating it
    Set objRevCutout = objModel.RevolvedCutouts.AddFinite(Profile:=objCutoutProfile, _
                                                          RefAxis:=objCutoutRefAxis, profileSide:=igLeft, ProfilePlaneSide:=igSymmetric, AngleOfRevolution:=(3 * PI / 4))
    objCutoutProfile.Visible = False
    If (objModel.RevolvedCutouts(1).Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the RevolvedCutouts object fails"
    End If
    ' getting the status of the revolved cutout feature
    lngStatus = objRevCutout.Status
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objLine = Nothing
    Set objRefAxis = Nothing
    Set objModel = Nothing
    Set objProfileArray(1) = Nothing
    Set objProfileArray(2) = Nothing
    Set objRevCutout = Nothing
    Set objCutoutProfile = Nothing
    Set objCutoutLine = Nothing
    Set objCutoutRefAxis = Nothing
End Sub