|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  EndCapsStatus | Sets and returns the end caps status for the referenced object. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelingModeType | Returns the modeling mode of the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Profile | Sets and returns the Profile object used to construct the referenced feature object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  SideFaces | Returns a collection of all the side faces for the referenced feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |