Solid Edge Part Type Library
BlendShapeValue Property
Description
Specifies the blend shape value.
Property type
Read-write property
Syntax
Visual Basic
Public Property BlendShapeValue As Double
Remarks
When the blend shape for the referenced Round object is igBlendShapeRatioChamfer or igBlendShapeConic, then BlendShapeValue can be any value greater than 0. When the blend shape for the referenced Round object is igBlendShapeG2Continuous, then BlendShapeValue can be any value greater than 0 and less than or equal to 10.
See Also

Round Object  | Round Members

Send comments on this topic.