Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    Dim objProfile As SolidEdgePart.Profile
    Dim objExtCutout As SolidEdgePart.ExtrudedCutout
    Dim objEdges As Object
    Dim objEdgeArray(1 To 1) As SolidEdgeGeometry.Edge
    Dim objRounds As SolidEdgePart.Rounds
    Dim objRound As SolidEdgePart.Round
    Dim dblRadiusArray(1 To 1) As Double
    Dim lngStatus As Long
    Const TESTFILE = "T:\vbtests\testcases\cube.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    Set objModel = objDoc.Models(1)
    ' *** Create a simple cutout
    ' Create a profile for the extruded cutout feature and validate it
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objProfile.Circles2d.AddByCenterRadius(x:=0.015, y:=0.015, Radius:=0.005)
    lngStatus = objProfile.End(ValidationCriteria:=igClosed)
    If lngStatus <> 0 Then
        MsgBox "Profile for the Extruded Cutout feature is not closed"
    End If
    ' Create the Extruded Cutout feature and validate it
    Set objExtCutout = objModel.ExtrudedCutouts.AddFinite(Profile:=objProfile, _
                                                          ProfileSide:=igLeft, ProfilePlaneSide:=igRight, Depth:=0.05)
    objProfile.Visible = False
    If objExtCutout.Status <> igFeatureOK Then
        MsgBox "AddFinite method of ExtrudedCutouts object failed"
    End If
    ' *** creating a simple round on a single edge
    ' defining the radius for rounding an edge
    Set objRounds = objModel.Rounds
    Set objEdges = objModel.ExtrudedProtrusions(1).Edges(edgetype:=igQueryAll)
    Set objEdgeArray(1) = objEdges(1)
    dblRadiusArray(1) = 0.005
    ' Create the round feature and validate it
    Set objRound = objRounds.Add(NumberOfEdgeSets:=1, EdgeSetArray:=objEdgeArray, _
                                 RadiusArray:=dblRadiusArray)
    If objRound.Status <> igFeatureOK Then
        MsgBox "Round feature failed"
    End If
    'Reorder the round feature ahead of cutout feature
    Call objRound.Reorder(TargetFeature:=objModel.Features(1), InsertBefore:=False)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModel = Nothing
    Set objEdges = Nothing
    Set objEdgeArray(1) = Nothing
    Set objRounds = Nothing
    Set objRound = Nothing
End Sub