Solid Edge Part Type Library
SlotEndCondition Property
Description
Property type
Read-write property
Syntax
Visual Basic
Public Property SlotEndCondition As FeaturePropertyConstants
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()

        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objSketchs As SolidEdgePart.Sketchs = Nothing
        Dim objSketch As SolidEdgePart.Sketch = Nothing
        Dim objProfile As SolidEdgePart.Profile = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objSlots As SolidEdgePart.Slots = Nothing
        Dim objSlot As SolidEdgePart.Slot = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            'set the modeling mode
            objPartDocument.ModelingMode = SolidEdgePart.ModelingModeConstants.seModelingModeOrdered

            objSketchs = objPartDocument.Sketches

            'get a sketch & profile
            objSketch = objSketchs.Item(1)
            objProfile = objSketch.Profile

            objModels = objPartDocument.Models
            objModel = objModels.Item(1)

            'get Slots collection
            objSlots = objModel.Slots

            'create a Slot
            objSlot = objSlots.Add(objProfile,
                                   SolidEdgePart.FeaturePropertyConstants.igRegularSlot,
                                   SolidEdgePart.FeaturePropertyConstants.igFormedEnd,
                                   0.005,
                                   0.0,
                                   0.0,
                                   SolidEdgePart.FeaturePropertyConstants.igFinite,
                                   SolidEdgePart.FeaturePropertyConstants.igLeft,
                                   0.5,
                                   SolidEdgePart.KeyPointExtentConstants.igTangentNormal,
                                   Nothing,
                                   SolidEdgePart.FeaturePropertyConstants.igNone,
                                   SolidEdgePart.FeaturePropertyConstants.igNone,
                                   0.0,
                                   SolidEdgePart.KeyPointExtentConstants.igTangentNormal,
                                   Nothing,
                                   Nothing,
                                   SolidEdgePart.OffsetSideConstants.seOffsetNone,
                                   0.0,
                                   Nothing,
                                   SolidEdgePart.OffsetSideConstants.seOffsetNone,
                                   0.0)

            'set some properties (edit) on the slot
            objSlot.SlotEndCondition = SolidEdgePart.FeaturePropertyConstants.igLancedEnd

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Slot Object  | Slot Members  | Solid Edge ST5 - What's New

Send comments on this topic.