|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BeadMaterialLength | Sets and returns the bead material length for the referenced StitchWeld object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  EndOffset | Sets and returns the length of material to remove from the end of the weld bead for the referenced StitchWeld object. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  GapLength | Sets and returns the gap length between solid portions of the bead for the referenced StitchWeld object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  StartOffset | Sets and returns the length of material to remove from the start of the weld bead for the referenced StitchWeld object. | 
|  Status | Returns the status of the specified object. | 
|  StitchWeldAnnotationFormat | Sets and returns the annotation format for the referenced StitchWeld object. | 
|  StitchWeldType | Sets and returns the stitch weld type for the referenced StitchWeld object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. |